S32 Design Studio for Power v1.1 license problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for Power v1.1 license problem

Jump to solution
4,532 Views
cst
Contributor II

We use the NXP S32 Design Studio (Power Architecture) v1.1 for development with the DEVKIT-MPC5748G.

The IDE stopped working with an licence error starting this year (2017).

173938_173938.pngS32IDE_E200_licence2.png

 

The licence is valid until 2020 according to the licence Information on our NXP account.

173937_173937.pngS32IDE_E200_licence.png

Additionally the Power Architecture version of the S32 Design Studio has vanished from the NXP download websites.

 

Is this just an error or has NXP stopped supporting the Power Architecture within S32 Design Studio?

1 Solution
4,099 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

could you please try to activate S32DS once again? It seems it works now.

Regards,

Martin

View solution in original post

0 Kudos
Reply
4 Replies
4,099 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

Thank you for the notice, we have already check the issue and we are working on it with the highest priority. We are very sorry for any inconvenience; we will try to fix the problem as soon as possible. I will keep you informed about the progress.

Regards,

Martin

0 Kudos
Reply
4,100 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

could you please try to activate S32DS once again? It seems it works now.

Regards,

Martin

0 Kudos
Reply
4,099 Views
cst
Contributor II

Hello Martin,

thank you very much for the swift resolution.

The license works now.

The only question that remains is, why the Power Architecture version of S32 Design Studio is missing from all links on the NXP websites. Is this also an error or is the version of S32DS not supported anymore?

Regards,

Christian

4,099 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

I do not know why S32DS for power is missing, but it is definitely a bug. It does not mean it is not supported anymore. I will try to find out where is the problem and I hope it will be resolved asap.

Regards,

Martin