S32 Design Studio for Power Architecture, Version 2017.R1 update patch failed.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for Power Architecture, Version 2017.R1 update patch failed.

2,053 Views
Zhangxq
Contributor I

when i update the software from the website.it will be show below trouble,CAN YOU HELP ME?An error occurred while collecting items to be installed
session context was:(profile=SDKProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=null --> [R]com.nxp.s32ds.cross.sdk.S32PA_1.8.0.brc_root 1.0.0.201811261458, action=).
The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.
The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.

 

Thanks

0 Kudos
Reply
1 Reply

2,032 Views
mikedoidge
NXP Employee
NXP Employee

Hello @Zhangxq,

I am unable to reproduce the issue. It is quite unusual.

Have you tried to reboot the machine and relaunch S32 Design Studio?

It is possible that some file had become corrupt. Try uninstalling and then reinstalling S32 Design Studio.

Best Regards,

Mike

0 Kudos
Reply