S32 Design Studio : Launching project Default (61%) Stall

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio : Launching project Default (61%) Stall

4,526件の閲覧回数
cholland
Contributor V

Hi,

For over a year, S32 Design Studio and PE Micro 'Multilink Universal' worked just fine.

Now, all of a sudden, S32 stalls at 61% for a very long time. Eventually it does reach 100%. Maybe after 5-10 minutes or so.

I don't know what could have happened. I moved the USB cables, but I moved them back.

I think there might have been a Windows Update. (I am using Windows 7) 

So now, I am trying to figure out the proper way to debug the issue.

It doesn't matter whether or not PE Micro 'Multilink Universal' is plugged in or not. It still sits at 61% for a long time.

1. I tried different hardware/projects, but that didn't make a difference.

2. I tried reinstalling PE Micro Drivers, but that didn't make a difference. 

3. I tried updating S32 Design Studio, but it's all up to date.

4. When I run pegdbserver stand-alone, it seems to startup up almost instantly.

Everything is working, it just takes a very long time.

I am going to keep mucking with it. I'll post results if and when I figure out what happened.

C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.5.
201807182113\win32>pegdbserver_power_console.exe -startserver -device=MPC5746C

P&E GDB Server for Power devices, Version 6.94.00.00
Copyright 2018, P&E Microcomputer Systems Inc, All rights reserved

Loading library C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gd
bjtag.ppc_1.7.5.201807182113\win32\gdi\unit_ngs_ppcnexus_internal.dll ... Done.

Command line arguments: -startserver -device=MPC5746C
Device selected is mpc5746c
HW Auto-Selected : Interface=USBMULTILINK Port=PEM16C71E ; USB1 : Multilink Un
iversal Rev C (PEM16C71E)
Connecting to target.
P&E Interface detected - Flash Version 9.81

Starting reset script (C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.d
ebug.gdbjtag.ppc_1.7.5.201807182113\win32\gdi\P&E\s32e200_mpc574xc.mac) ...
REM This script is compatible with MPC574xC devices.


REM Clean GPRs to remove residual data after using algorithm


REM Initialize all of the Main SRAM - 512KB


Initializing RAM from $40000000 to $4007FFFF.

Reset script (C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbj
tag.ppc_1.7.5.201807182113\win32\gdi\P&E\s32e200_mpc574xc.mac) completed.

MPC574xB/C/D Device detected.
Device is mpc5746c.
Mode is In-Circuit Debug.

(C)opyright 2012, P&E Microcomputer Systems, Inc. (www.pemicro.com)
API version is 101

Server 1 running on 127.0.0.1:7224
Server 2 running on 127.0.0.1:7226
Server 3 running on 127.0.0.1:7228
Server 4 running on 127.0.0.1:7230
Server 5 running on 127.0.0.1:7232
Server 6 running on 127.0.0.1:7234
Server 7 running on 127.0.0.1:7236
Server 8 running on 127.0.0.1:7238
Server 9 running on 127.0.0.1:7240
Server 10 running on 127.0.0.1:7242
All Servers Running

0 件の賞賛
返信
2 返答(返信)

3,719件の閲覧回数
cholland
Contributor V

I reinstalled S32 Design Studio.

I think there might be a problem with the firewall. It seemed to work when we disabled it.

It works when we try another computer. The PE Micro Multilink Universal is working correctly.

Sometimes it never starts, with this error message.

An internal error occurred during: "Start GDB Server Job".
RequestMonitor: Sequence "", result for executing step #0 = Status CANCEL: org.eclipse.cdt.dsf code=10005
Composite status null children=[Status CANCEL: com.pemicro.debug.gdbjtag.ppc code=1 PEmicro GDB Launch Failure :
The GDB Server was not able to establish a connection to the target processor.
Please check your connections and power.
Verify that the launch settings in the Debug Configuration are accurate.
null Status ERROR: org.eclipse.cdt.dsf code=10005 Request for monitor: 'RequestMonitor (com.pemicro.debug.gdbjtag.ppc.Backend$GdbServerStep$1@170107b):
Status CANCEL: com.pemicro.debug.gdbjtag.ppc code=1 PEmicro GDB Launch Failure : The GDB Server was not able to establish a connection to the target processor.
Please check your connections and power. Verify that the launch settings in the Debug Configuration are accurate.
null' resulted in a rejected execution exception. null], done() method called more than once

0 件の賞賛
返信

3,719件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello [email protected]‌,

Perhaps you should report this to P&E Micro. The issue certainly seems to be related to their products.

This may not apply to the MPC5746C, but it may be worth a try. There is a known issue with communication speed on older parts and the newer P&E Multilinks: https://community.nxp.com/docs/DOC-340911 

Hope it helps,

Mike

0 件の賞賛
返信