S32 Debug Probe not able to load .elf

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Debug Probe not able to load .elf

1,771 Views
Kadadi
Contributor I

Hi ,

I am able to compile the FlexCan application from S32Design Studio but when I try to load using S32 Debug Probe facing issue. 
Please find the below screenshot of the error which I am facing.

Kitti_0-1722952589135.png

 

Please let me know if any configuration is missing from myside.

Thanks,

Krishna K

0 Kudos
Reply
3 Replies

1,643 Views
stanish
NXP Employee
NXP Employee

Hello,

1) let me ask you which version of S32 Design studio are you using?

I'd strongly recommend you install the latest update #13 

stanish_0-1723478274432.png

Please go to installed software and check S32Z2/E2 Development package version

stanish_1-1723478333572.png

or alternatively you can check it in S32DS Extension and updates:

stanish_2-1723478436158.png

2) Which board are you targeting? Is it NXP one e.g. S32Z27x - DC (Daughter Card) ?

3) Which S32 Debug probe interface are you using (USB or Ethernet)? Is TX/RX led blinking green when you connect the probe to the board?

4) Have you been able to connect to any other device using S32DebugProbe?

5) Can I ask you where you get the example code you are trying to build and debug?

This will help to address the loading issue much faster.

Thanks,

Stan

0 Kudos
Reply

1,743 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

S32Z/E is still in preproduction, for which for all information/support help us contacting your local NXP FAE/DFAE/representative.

We do apologize for the inconvenience.

Please, let us know.

0 Kudos
Reply

1,766 Views
Kadadi
Contributor I

Board : S32Z277
Core : M33 Core 0

 

0 Kudos
Reply