S32 DS debugger cant register

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 DS debugger cant register

1,592件の閲覧回数
Kunal_Gupta
NXP Employee
NXP Employee

Hi all,

I am using S32DS and having S32K312-EVB board. Running the port example sketch, but during the debug configuration it asks for registration. But on doing so, error like this comes up:

What is the solution for it? I have installed the software again, have make sure that all relevant drivers are installed.

 

Would be looking for reply as early as possible.

 

 

0 件の賞賛
返信
1 返信

1,569件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @Kunal_Gupta, 

You do not need to register with P&E. This only enables them to have your email address to contact you with product notifications, etc. There is no impact to your ability to use S32 Design Studio or the P&E GDB debugger. It also does not impact the support you receive from NXP or P&E.

The error appears to indicate the Eclipse environment is unable to access the internet to load the P&E registration page.

For further questions on this, I would suggest that you contact P&E Micro.

Best Regards,

Mike

0 件の賞賛
返信