S32 DS debugger cant register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 DS debugger cant register

1,599 Views
Kunal_Gupta
NXP Employee
NXP Employee

Hi all,

I am using S32DS and having S32K312-EVB board. Running the port example sketch, but during the debug configuration it asks for registration. But on doing so, error like this comes up:

What is the solution for it? I have installed the software again, have make sure that all relevant drivers are installed.

 

Would be looking for reply as early as possible.

 

 

0 Kudos
Reply
1 Reply

1,576 Views
mikedoidge
NXP Employee
NXP Employee

Hello @Kunal_Gupta, 

You do not need to register with P&E. This only enables them to have your email address to contact you with product notifications, etc. There is no impact to your ability to use S32 Design Studio or the P&E GDB debugger. It also does not impact the support you receive from NXP or P&E.

The error appears to indicate the Eclipse environment is unable to access the internet to load the P&E registration page.

For further questions on this, I would suggest that you contact P&E Micro.

Best Regards,

Mike

0 Kudos
Reply