S32 DS V2.1, MPC5746R, several C file can't be compiled.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 DS V2.1, MPC5746R, several C file can't be compiled.

1,771 Views
ZhouYiChuan
Contributor III

Dear NXP experts:

Could you do me a favor to support me on this S32 Design Studio issue?

the MCU is MPC5746R, S32 Design Studio V2.1, the  CORE0 project  can be built successfully. 

But forCORE1 project , there're following Errors, and no hint to fix:

1) several files can't be built

2) files like flashrchw.c, main_Z4_1.c can't be added into build path-debug, there is a '/'

S32_MPC5746R_Issue.png

 

thanks and BR

YiChuan

Tags (1)
0 Kudos
Reply
4 Replies

1,769 Views
ZhouYiChuan
Contributor III

PS: 

there is no hint for the errors in files like BTS.c , FS6500.c etc, only a simple error description in the snapshot  is provided by S32. 

0 Kudos
Reply

1,759 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share output from build console? 

 

Jiri 

0 Kudos
Reply

1,694 Views
ZhouYiChuan
Contributor III

Hi, Jiri:

There is some issue in the output built from newly created MPC5746R project .

So , could you please support me on the building issue of older 5746R project. 

the console is below:

S32DS_Console.PNG

thanks and BR

YiChuan

0 Kudos
Reply

1,744 Views
ZhouYiChuan
Contributor III

Hello Jiri:

After I created new MPC 5746R projects and merged the codes into new projects, the issue was resolved.

Maybe the reason is the old projects was created with different S32 DS version. 

Anyway, thanks a lot !!

 

BR

YiChuan