S32 DS V2.1, MPC5746R, several C file can't be compiled.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 DS V2.1, MPC5746R, several C file can't be compiled.

1,752件の閲覧回数
ZhouYiChuan
Contributor III

Dear NXP experts:

Could you do me a favor to support me on this S32 Design Studio issue?

the MCU is MPC5746R, S32 Design Studio V2.1, the  CORE0 project  can be built successfully. 

But forCORE1 project , there're following Errors, and no hint to fix:

1) several files can't be built

2) files like flashrchw.c, main_Z4_1.c can't be added into build path-debug, there is a '/'

S32_MPC5746R_Issue.png

 

thanks and BR

YiChuan

タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,750件の閲覧回数
ZhouYiChuan
Contributor III

PS: 

there is no hint for the errors in files like BTS.c , FS6500.c etc, only a simple error description in the snapshot  is provided by S32. 

0 件の賞賛
返信

1,740件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share output from build console? 

 

Jiri 

0 件の賞賛
返信

1,675件の閲覧回数
ZhouYiChuan
Contributor III

Hi, Jiri:

There is some issue in the output built from newly created MPC5746R project .

So , could you please support me on the building issue of older 5746R project. 

the console is below:

S32DS_Console.PNG

thanks and BR

YiChuan

0 件の賞賛
返信

1,725件の閲覧回数
ZhouYiChuan
Contributor III

Hello Jiri:

After I created new MPC 5746R projects and merged the codes into new projects, the issue was resolved.

Maybe the reason is the old projects was created with different S32 DS version. 

Anyway, thanks a lot !!

 

BR

YiChuan