S32 Check value of variables

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Check value of variables

3,273 Views
qiaodeng
Contributor II

Hi every body,

    I can't see any variable in the variables window. I want to check the value of some variables, but when I tried  to add them to the expression window, they didn't show , and the software often encounter a problem of no response.

155429_155429.pngpastedImage_0.png

     What is the correct way to check the value of variables? Any tips would be highly appreciated.

 

Best Regards

Qiao

Labels (2)
0 Kudos
Reply
3 Replies

2,760 Views
xuantruongdao
NXP Employee
NXP Employee

Sometime this problem occurs. You can see in debugger view, it is not displayed fully. You should terminate and debug again and recheck. Hope to help you.

0 Kudos
Reply

2,760 Views
qiaodeng
Contributor II

pastedImage_0.png

    I still can't see any variable or register...Have you ever encountered this situation?

0 Kudos
Reply

2,760 Views
stanish
NXP Employee
NXP Employee

Hi,

Unfortunately S32DS cannot display/update neither a variable nor peripheral register while the target is running.

You should suspend the execution first and then check the "Expressions/EmbSysReg" Views.

Stan

0 Kudos
Reply