The same project is ok in my colleague's computer. But in my computer, it reports an err " ewl_c.specs: No such file or directory"
can anyone help me to solve it? Thank you very much!
Hi,
have you tried to "Clean" and rebuild your project?
Which version+Build number does your workmate has? The version you have is the first official release available.
I suspect your colleague uses a non-official release and therefore you might experience some compatibility issues.
I'd encourage you to use official release in order to avoid such a problems.
Regards,
Stan
I find i just delete the err message and then rebuild the project, it's OK! :smileyshocked:
Now i have another question(see below)
Building file: ../source/srv/sys/osv/osv.c
Executing target #1 ../source/srv/sys/osv/osv.c
Invoking: Standard S32DS C Compiler
powerpc-eabivle-gcc "@source/srv/sys/osv/osv.args" -MMD -MP -MF"source/srv/sys/osv/osv.d" -MT"source/srv/sys/osv/osv.o" -c -o "source/srv/sys/osv/osv.o" "../source/srv/sys/osv/osv.c"
powerpc-eabivle-gcc.exe: fatal error: C:/Freescale/S32_Power_v1.0/S32DS/e200_ewl2/lib/ewl_c.specs: attempt to rename spec 'cpp_unique_options' to already defined spec 'old_cpp_unique_options'
compilation terminated.
make: *** [source/srv/sys/osv/osv.o] Error 1
This is caused by different versions of S32. My workmate has low version of S32, mine is high version(you can see in the picture above). Every time i copy his project to my computer, it reports the err above, could you help me for this? Thank you very much!
 
					
				
		
 martin_kovar
		
			martin_kovar
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
could you please share Compiler, Linker and Assembler settings (see following screen)?
Regards,
Martin
Hello,
Could you please check if --sysroot path matches with your environment (see the screenshot below) and if your S32DS directory includes this folder/file too (perhaps the installation of S32DS was not completed).
Stan
 
					
				
		
 martin_kovar
		
			martin_kovar
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
could you please provide me another information about your problem?
1) Which S32 Design Studio you use? For ARM or for Power architecture?
2) Which processor you use?
3) Does your colleague have the same operating system?
4) Which module/file is the error in?
5) Do you include some external (our own) libraries?
6) Are you able to create new empty project and compile it successful?
Regards,
Martin