Resources not available (barred) in New project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Resources not available (barred) in New project

2,004 次查看
AdrianR
NXP Employee
NXP Employee

When creating a new SDK project for S32K144, the ProcessorExpert and other items appear barred (NA).

pastedImage_1.png

While the other resources are easy to add using the Build configuration explorer, the PE item cannot be added and remains barred.

pastedImage_2.png

This is not the same if I open New project from Example... There PE is included ok.

This is more a cosmetic issue as I am able to configure, compile, etc.

I'm using latest version as of today:

C/C++ Development Tools 9.2.1.201703062208
C/C++ GCC Cross Compiler Support 9.2.1.201703062208
C/C++ GDB Hardware Debugging 9.2.1.201703062208
C/C++ Memory View Enhancements 9.2.1.201703062208
CDT GNU Debug Patch 1.0.0
CDT Platform Patch 1.0.1
Eclipse Platform 4.6.3.M20170301-0400
Eclipse XML Editors and Tools 3.8.2.v201702270442
Embedded Systems Register View (SFR) 1.0.0.201707191349
FreeRTOS Task Aware Debugger for GDB 1.0.1.201610061345
FSL Eclipse Updater Custom Actions Feature for Eclipse 4.4.x 2.0.12.FSL_150303
Git integration for Eclipse 4.10.0.201712302008-r
GNU ARM C/C++ J-Link Debugging 4.1.2.201701141320
GNU ARM PEMicro Interface Debugging Support 3.1.1.201708081924
IAR C-SPY Debug Support for ARM 7.20.0.201801101216
IAR Common Components 2.0.0.201801101216
IAR Common Debugger Components 1.0.0.201801101216
IAR Plugin Manager 1.0.0.201706271353
IAR Toolchain for ARM 7.20.0.201801101216
Java implementation of Git 4.10.0.201712302008-r
MQX RTOS Task Aware Debugger for GDB 1.0.9.201707031831
Processor Expert for S32 Design Studio 1.1.0.RT7_b1743-0713
S32 Design Studio ARM Cortex-A Toolchain 1.0.0.201708101436
S32 Design Studio ARM Cortex-M Toolchain 1.0.0.201708101436
S32 Design Studio Example Projects 1.0.0.201709280936
S32 Design Studio Examples 1.0.0.201707191435
S32 Design Studio for ARM 1.0.0.201708101436
S32 Design Studio for ARM Win32 Update 0.0.1
S32 Design Studio for ARM, Version 2.0. Documentation 2.0.0.201708091545
S32 Design Studio FreeMASTER SDK 1.0.0.201708101254
S32 Design Studio GNU 1.0.0.201708101433
S32 Design Studio KEAx AMMCLIB SDK 1.0.0.201708101254
S32 Design Studio MAC57D5xx support 1.0.0.201708101436
S32 Design Studio MQX 4.2 Halo 0.6 Example Projects 1.0.0.201709280936
S32 Design Studio OS Awareness for ARM architecture 1.0.0.201707191351
S32 Design Studio Platform 1.0.0.201707191435
S32 Design Studio s32k142 support 1.0.0.201711151036
S32 Design Studio s32k146 support 1.0.0.201711151036
S32 Design Studio s32k148 support 1.0.0.201711151036
S32 Design Studio S32K14x EAR SDK 1.0.0.201708101254
S32 Design Studio S32K14x EAR SDK 0.8.6 1.0.0.201712081731
S32 Design Studio S32K14x SDK 0.8.5 EAR 1.0.0.201709281950
S32 Design Studio S32K14x_AMMCLIB SDK 1.0.0.201708101254
S32 Design Studio S32K1xx support 1.0.0.201711151036
S32 Design Studio S32V common support 1.0.0.201708101436
S32 Design Studio S32V support 1.0.0.201708101436
S32 Design Studio SDK extension 1.0.0.201708101436
S32 KEAx SDK 1.0.0 1.0.0.201708101254

标记 (2)
0 项奖励
回复
1 回复

1,666 次查看
gearhead1107
Contributor IV

They're supposed to look like that :smileyhappy:

It's Eclipse's way of showing they're not part of the build

Icon and Label Decorators in Eclipse | MCU on Eclipse 

0 项奖励
回复