Reset cycle

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reset cycle

2,950件の閲覧回数
vladstoica
Contributor III

Hello,

 

I write some wrong code in flash and my evb is in cycle reset. How do I get out from this reset with S32 design studio(D1 is always lighted).

 

Thanks,

 

Vlad

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,705件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi Vlad,

you forgot to write two important points. First point is the micro you use. Second point is the code you have flashed. Please clarify.

Regards,

Martin

0 件の賞賛
返信

2,705件の閲覧回数
vladstoica
Contributor III

Hi,

I use a MPC5748G with P&E p&e micro multilink usb. I flashed a code which modifies the flash memory(I modified the startup.s code and mem.ld) am probably that is the problem.

0 件の賞賛
返信

2,705件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi Vlad,

I do not think this should causes the problem. I suppose you looked at this thread https://community.nxp.com/thread/386055

Have you configured FCCU or you just changed startup and linker file?

Could you please send me a screen of the error, which you get from S32DS?

Regards,

Martin

0 件の賞賛
返信