Reset cycle

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reset cycle

2,220 次查看
vladstoica
Contributor III

Hello,

 

I write some wrong code in flash and my evb is in cycle reset. How do I get out from this reset with S32 design studio(D1 is always lighted).

 

Thanks,

 

Vlad

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

1,975 次查看
martin_kovar
NXP Employee
NXP Employee

Hi Vlad,

you forgot to write two important points. First point is the micro you use. Second point is the code you have flashed. Please clarify.

Regards,

Martin

0 项奖励
回复

1,975 次查看
vladstoica
Contributor III

Hi,

I use a MPC5748G with P&E p&e micro multilink usb. I flashed a code which modifies the flash memory(I modified the startup.s code and mem.ld) am probably that is the problem.

0 项奖励
回复

1,975 次查看
martin_kovar
NXP Employee
NXP Employee

Hi Vlad,

I do not think this should causes the problem. I suppose you looked at this thread https://community.nxp.com/thread/386055

Have you configured FCCU or you just changed startup and linker file?

Could you please send me a screen of the error, which you get from S32DS?

Regards,

Martin

0 项奖励
回复