Regarding Export the SDK Example code to IAR EWARM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding Export the SDK Example code to IAR EWARM

2,082 次查看
leekate-b45752
NXP Employee
NXP Employee

Hello Team, 

I can export the project file without SDK v0.8.6 to IAR EWARM, but I couldn't export SDK example project file. 

Could guide about it?

I'm using S32 DS 2018 R1, and IAR EWARM v8.22.1

Best regards,

Kate Lee

标签 (3)
0 项奖励
回复
1 回复

1,715 次查看
stanish
NXP Employee
NXP Employee

Hi Kate,

Which specific example do you mean?

AFAIK the most examples are available only for Standard s32DS GCC toolchain.

Anyway there is one example - Hello World for IAR EWARM

pastedImage_1.png

This one you can directly open in IAR EWARM (see below).

pastedImage_2.png

Hope it helps...

Stan

0 项奖励
回复