Re-Flash issue with S32 Flash tool for S32V234

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re-Flash issue with S32 Flash tool for S32V234

1,480件の閲覧回数
johnyoo
NXP Employee
NXP Employee

Hello,

I'm trying to flash u-boot into eMMC and I got the issue that fail to load algorithm and device file when I reprogramming it.

There was no issue to flash u-boot at the first time, however, the issue was occurred on second time, it means that flash tool doesn't work after running u-boot.

Could you explain the reason why it doesn't work after running u-boot and solution?

I know the workaround in case of using EVB with switching boot device jumper to avoid booting, however, customer board has no jumper to prevent booting. 

pastedImage_2.png

It seems that it is same issue when running the demo sdhc_fatfs_s32v234. The demo doesn't work if u-boot is in the SDCARD.

1. Please explain root cause of the issue.

2. How can I modify the sdhc_fatfs_s32v234 demo to run with SDCARD u-boot inside.

Thank you.

Best Regards,

John Yoo

ラベル(1)
タグ(3)
0 件の賞賛
返信
0 返答(返信)