Rappid Bootloader Erase and program option

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Rappid Bootloader Erase and program option

2,045件の閲覧回数
prathapvc
Contributor III

While flashing the application code using .s19 file by selecting "erase and program" option in Rappid Bootloader utility i found that the bootloader erases all 31 blocks of flash memory in MPC5777C

So can you suggest whether we can store the data in EEPROM Data block (0x00030000 - 0x0003FFFF) or UTEST block (0x00400000 - 0x00403FFF) in flash memory through JTAG probe which is not supposed to be erased by RappID Bootloader.

0 件の賞賛
返信
1 返信

1,195件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello,

Indeed RappID Bootloader erases entire program flash memory.

If you program Dflash/Utest flash block via JTAG these blocks are NOT erased by the RappID bootlader.

Hope it helps.

Stan

0 件の賞賛
返信