RTD install fails on S32DS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RTD install fails on S32DS

1,275 次查看
AdrianR
NXP Employee
NXP Employee

I have the attached error log when trying to install (latest) RTDs on top of S32DS 3.6 (Windows). I have also one similar error log from a customer using the same setup, on Linux.

The attached log is from installing:

SW32K1_S32M24x_RTD_R21-11_3.0.0_D2503_DesignStudio_updatesite.zip

I also uninstalled the previous RTD that was working fine, and try to re-install the same, and I ran into the same error.

Previous RTD, not installing anymore: 

SW32K1_S32M24x_RTD_R21-11_2.0.0_P04_D2404_DS_updatesite.zip

 

My installation:
Package: S32Z2/E2 development package; Version: 3.6.0; Build id: 202411272150
Package: S32K1xx development package; Version: 3.6.0; Build id: 202411272151
Package: S32N5 FreeMASTER Serial Communication Driver; Version: 1.4.2; Build id: 202412100818
Package: S32R41 development package; Version: 3.6.0; Build id: 202411272147
Package: NXP GCC for Arm Embedded Processors v10.2 build 1728; Version: 1728; Build id: 202411051359
Package: S32M2xx development package; Version: 3.6.0; Build id: 202411272146
Package: GDB Client for Arm Embedded Processors 15.1 Build 1703; Version: 1703; Build id: 202411211023
Package: S32N5 development package; Version: 3.6.0; Build id: 202411281414
Package: S32G development package; Version: 3.6.0; Build id: 202411272150
Package: S32R45 development package; Version: 3.6.0; Build id: 202411272146
Package: S32 Design Studio Platform Tools package; Version: 3.6.0; Build id: 202411280504
Package: NXP GCC for Arm Embedded Processors v11.4 build 1763; Version: 1763; Build id: 202411051318
Package: S32 Design Studio Debugger Core; Version: 3.6.0; Build id: 202411280422
Package: S32K3XX Real-Time Drivers AUTOSAR R21-11 Version 5.0.0; Version: 5.0.0; Build id: 202410011049
Package: S32 Design Studio Platform package; Version: 3.6.0; Build id: 202411280504
Package: S32K3xx development package; Version: 3.6.0; Build id: 202411272154
Package: S32M27X Real-Time Drivers AUTOSAR R21-11 Version 5.0.0; Version: 5.0.0; Build id: 202410011049
Package: S32K3_S32M27x Real-Time Drivers AUTOSAR R21-11 Version 5.0.0; Version: 5.0.0; Build id: 202410011049
Package: NXP GCC for Arm Embedded Processors v9.2 build 1649; Version: 1649; Build id: 202411051417
Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.9.5; Build id: 202412131551
Package: S32K39X Real-Time Drivers AUTOSAR R21-11 Version 5.0.0; Version: 5.0.0; Build id: 202410011049

标签 (1)
0 项奖励
回复
2 回复数

1,211 次查看
jiri_kral
NXP Employee
NXP Employee

Hi Adrian, 

I checked it on my side and it works without issue. Only difference which I found is that I have installed Configuration Tool - here are my installation details: 

 

Package: S32 Design Studio Platform package; Version: 3.6.0; Build id: 202411280504
Package: S32Z2/E2 development package; Version: 3.6.0; Build id: 202411272150
Package: S32K1xx development package; Version: 3.6.0; Build id: 202411272151
Package: S32 Configuration Tools R1.8 NPI data package for S32K3; Version: 1.8.0; Build id: 202411250824
Package: S32K3xx development package; Version: 3.6.0; Build id: 202411272154
Package: S32R41 development package; Version: 3.6.0; Build id: 202411272147
Package: NXP GCC for Arm Embedded Processors v10.2 build 1728; Version: 1728; Build id: 202411051359
Package: S32M2xx development package; Version: 3.6.0; Build id: 202411272146
Package: S32K3_S32M27x Real-Time Drivers AUTOSAR R21-11 Version 5.0.0; Version: 5.0.0; Build id: 202410011049
Package: GDB Client for Arm Embedded Processors 15.1 Build 1703; Version: 1703; Build id: 202411211023
Package: S32 Configuration Tools Package; Version: 1.8.1; Build id: 202502251421
Package: S32K1_S32M24X Real-Time Drivers AUTOSAR R21-11 Version 3.0.0; Version: 3.0.0; Build id: 202503210207
Package: S32G development package; Version: 3.6.0; Build id: 202411272150
Package: S32R45 development package; Version: 3.6.0; Build id: 202411272146
Package: NXP GCC for Arm Embedded Processors v9.2 build 1649; Version: 1649; Build id: 202411051417
Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.9.5; Build id: 202412131551
Package: S32 Design Studio Platform Tools package; Version: 3.6.0; Build id: 202411280504
Package: NXP GCC for Arm Embedded Processors v11.4 build 1763; Version: 1763; Build id: 202411051318
Package: S32 Design Studio Debugger Core; Version: 3.6.0; Build id: 202411280422
Package: S32K3XX Real-Time Drivers AUTOSAR R21-11 Version 5.0.0; Version: 5.0.0; Build id: 202410011049

0 项奖励
回复

1,246 次查看
ola_gook
Contributor III

Same problem with SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.zip
Does not install under DS3.6

Errors start with:
An error occurred while collecting items to be installed
session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
No repository found containing: osgi.bundle,com.nxp.kex.standalone,1.0.0.202502251351
No repository found containing: osgi.bundle,com.nxp.s32ds.cle.uct,1.0.0.202502251421
No repository found containing: osgi.bundle,com.nxp.s32ds.cle.uct.core,1.0.0.202502251421
No repository found containing: osgi.bundle,com.nxp.s32ds.cle.uct.migration,1.0.0.202502251421

0 项奖励
回复