Question marks after moving folder

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question marks after moving folder

ソリューションへジャンプ
4,510件の閲覧回数
roy_vanlierop
Contributor III

The new Project Wizard doesn't like spaces. I created a project and moved it to to the filepath with spaces. Now the folders have a question mark. How do I remove these?

The Project juist cleans/builds fine and there seems to be nothing wrong. 

roy_vanlierop_0-1644496504646.png

40% of development is struggling with the IDE...

0 件の賞賛
返信
1 解決策
4,500件の閲覧回数
roy_vanlierop
Contributor III

Found the problem: 

The folder I moved the project to is a GIT folder so I just had to commit to remove the question marks. 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,496件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share more details about your approach? 

S32DS is based on Eclipse and Eclipse can't handle spaces in project name/path because of it is a multiplatform IDE (there is different way of handling  spaces, back slash and other characters on Unix Like and Windows OS). That's why you can't create project/ with spaces and other special characters. 

 

Jiri

0 件の賞賛
返信
4,501件の閲覧回数
roy_vanlierop
Contributor III

Found the problem: 

The folder I moved the project to is a GIT folder so I just had to commit to remove the question marks. 

0 件の賞賛
返信