Question about update install failure S32DS_ARM_v2018.R1_UP*.zip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about update install failure S32DS_ARM_v2018.R1_UP*.zip

ソリューションへジャンプ
4,534件の閲覧回数
jm_shin
Contributor I

Hello

I updated the S32DS along the guide page. (HOWTO: Update S32 Design Studio )
However, Problems will occur when installing S32DS_ARM_v2018.R1_UP*.zip.(update 1,8,9,10)

Whenever i perform an update, the 'freescale semiconductor' message appears.

If i select ok, an error will occur in S32DS.

If i select cancel, it can not update.

Problem Scenario

1) offline installation

Help" -> "Install New Software..." -> S32DS_ARM_v2018.R1_UP10

pastedImage_3.png

2) install start

pastedImage_4.png

3) 'freescale semiconductor' message appears.

pastedImage_5.png

4) If it select cancel

pastedImage_6.png

 

If there is a solution, please share it.

Thanks

タグ(2)
0 件の賞賛
返信
1 解決策
4,332件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I tried the same scenario - and for me is offline update working okay. You can try fresh install of S32DS and then apply update 10. 

Jiri

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,502件の閲覧回数
nirmal_masilamani
Contributor V

hello @jiri_kral ,

while installing S32DS_ARM_v2018.R1_UP*.zip, i am facing error.

An error occurred while collecting items to be installed
session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=null --> [R]com.nxp.s32ds.cross.sdk.S32K11x_AMMCLIB_1.1.13_root 1.0.0.201808151544, action=).
The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.
The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.

 

please provide me solution to resolve this.

0 件の賞賛
返信
4,333件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I tried the same scenario - and for me is offline update working okay. You can try fresh install of S32DS and then apply update 10. 

Jiri

0 件の賞賛
返信
4,331件の閲覧回数
jm_shin
Contributor I

Dear Jiri Kral

Thank you for answer.

0 件の賞賛
返信