Package install issue.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Package install issue.

1,550 Views
JIBIN_7
Contributor II

Attempting to install package, which is not being installed for NXP S32K312 3.0.0 SDK.

JIBIN_7_0-1708327953653.png 

but the result showing is Your original request has been modified.
"RTD S32M276.P01" will be ignored because a newer version is already installed.
"RTD S32K3.P01" will be ignored because a newer version is already installed.
"RTD S32K3XX.P01" will be ignored because a newer version is already installed.
"RTD S32K3.P01" will be ignored because a newer version is already installed.
"RTD S32K3XX.P01" will be ignored because a newer version is already installed.
"RTD S32K396.P01" will be ignored because a newer version is already installed.
Cannot complete the install because one or more required items could not be found.
Software being installed: RTD S32M276.P01 3.0.0.202304031555 (com.nxp.RTD.S32M276.P01.root.feature.feature.group 3.0.0.202304031555)
Missing requirement: RTD S32M276.P01 3.0.0.202304031555 (com.nxp.RTD.S32M276.P01.root.feature.feature.group 3.0.0.202304031555) requires 'org.eclipse.equinox.p2.iu; com.nxp.s32ds.s32m2.dev.feature.feature.group 1.0.0' but it could not be found

 

JIBIN_7_1-1708328071890.png

how can it solve this issue? 

i need to work in 3.0.0 packages.Im getting error ,when i attach 3.0.0 sdk .

But the code is working fine with 2.0.1 package sdk.

how to make the code working in 3.0.0.. Is that installation error or anything else?

 

 

 

0 Kudos
Reply
3 Replies

1,536 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @JIBIN_7 

To install the RTD drivers for S32K312 devices, you do not need to install the package for S32M276 devices.

If you also want to install the RTDs for these devices, please make sure to have installed the corresponding development package. 

Also, if you have the latest RTD releases and you want to use specifically version 3.0.0 P01, uninstall them because S32DS uses the latest release instead of the latest install. 

 

B.R.

VaneB

0 Kudos
Reply

1,459 Views
JIBIN_7
Contributor II

JIBIN_7_0-1709805986850.png

The above screenshot attached is from my colleagues laptop, we have installed same packages,but for me

JIBIN_7_1-1709806096589.png

kindly reply the solution asap.

there's a difference in Port pin Mscr and port pin level, value slew rate , port pin  direction

 

0 Kudos
Reply

1,457 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @JIBIN_7 

Check the following community post. It has information related to this error that should be useful for you.

S32K344 Port Configuration Problem

0 Kudos
Reply