NXP SBC-S32V234 Webserver interface with flutter App

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP SBC-S32V234 Webserver interface with flutter App

1,833 次查看
shraddhaben_m_j
Contributor I

Hello Everyone,


I am developing client application using flutter frame work to communicate with NXP webserver. In mobile app i am using websocket protocol to establish communication with NXP webserver . As I have client code in flutter is able to connect other server but it gives an error only when i am trying to connect NXP webserver . In client code the package i am using is web_socket_channel and it supports websocket secure connection(wss). So i want to know if there is updated NXP Webserever code is available with the websocket secure connection or anyone have updated server code wchi supports wss.


Error while try to connect NXP Webserver:
WebsocketException: Connection to 'http://10.5.11.88:7777#' was not upgraded to websocket.

Does anybody facing same issue?  It would be great help if i will find solution from you.

I have tried all the possible solution which is available online(websocket not upgraded error · Issue #11444 · flutter/flutter · GitHub )

Here is my Error Log and client code: flutter - Unhandled Exception: WebSocketException: Connection to 'http://10.5.11.88:7777/socketclust... 

Regards,

Shraddha

标记 (1)
0 项奖励
回复
1 回复

1,758 次查看
bpe
NXP Employee
NXP Employee

Please be aware, that support to S23V234 processor and related VSDK/BSP software is provided

only via tickets. You do already have an open ticket with a similar question which is assigned to

the approptiate support team. Please use that ticket to communicate with NXP Technical Support

with respect to your inquiry.

Regards,

Platon

0 项奖励
回复