NXP-HVBMS 400V TPL .mex file not opening error in S32DS v3.4 IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP-HVBMS 400V TPL .mex file not opening error in S32DS v3.4 IDE

1,770 Views
rushabhanadkar
Contributor I

I am facing this issue that whenever I am trying to open .mex file it is showing this error:

-> Platform SDK_S32K3_2022_03 version not supported by current version of the tool

My current setup is as follows:

1.S32K Design Studio v3.4

2.SW32K3_S32DS_3.4.3_D2112

The mex file is of the firmware version v0.9.1  : 

SW32K344_HVBMS-RD_Bring-up_Example_S32DS_0_9_1_D2303

directory :

->/HvBms400_Bring_up_examples/HvBms400_775_772_TPL_Bring_up/HVBMS-RD_Bring-up_example_S32DS.mex

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,723 Views
rushabhanadkar
Contributor I

The issue got solved by adding this zip file

SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204

Now I am able to open the HVBMS-RD_Bring-up_example_S32DS.mex file.

0 Kudos
Reply

1,738 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @rushabhanadkar 

Could you double-check if the SW32K3_RTD_4.4_2.0.0_D2203 is correctly installed in S32DS? To check this, go to S32DS Extension and Updates, and the software needs to say "Installed" as shown in the attached image. 

VaneB_0-1701975827086.png

 

B.R.

VaneB