I have installed the S32 design studio v 3.5 to work with SK32K312 microcontroller and need to install the extension/update of S32k3xx RTC v3.0.0
The installation seems to proceed but it is not successful the Reason shown is that there is a missing requirement, but I don't know how to get that requirement.
已解决! 转到解答。
Hi
Please offline install it by refer to HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------