Missing NXP GCC 10.2 in S32K3 Development Pack for S32 Design Studio 3.6.7 RFP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing NXP GCC 10.2 in S32K3 Development Pack for S32 Design Studio 3.6.7 RFP

Jump to solution
811 Views
Torris
Contributor I

According to the release note, the S32K3xx Development Package 3.6.7 RFP contains GCC version 11.4, 10.2.0 and 9.4.0.

However, after installation(SW32_S32DS_3.6.7_RFP_D2604_win32.x86_64.exe), there is only GCC version 11.4, no 10.2.0 and 9.4.0.

 

In S32DS Extensions and Updates, I can also only see GCC 11.4. There are no options for GCC 10.2.0 or GCC 9.4.

My operation system is Windows 10 x64 22H2. I am using an offline computer. I am not sure if that is the cause.

Labels (1)
0 Kudos
Reply
1 Solution
789 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

After installing S32 Design Studio 3.6.7 RFP on Windows 11, I found that I also needed to select and install "NXP GCC for Arm Embedded Processors v10.2 build 1728" in S32DS Extensions and Updates.

NXP GCC for Arm Embedded Processors v10.2 build 1728.pngSorry for the inconvenience we bring you!


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
790 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

After installing S32 Design Studio 3.6.7 RFP on Windows 11, I found that I also needed to select and install "NXP GCC for Arm Embedded Processors v10.2 build 1728" in S32DS Extensions and Updates.

NXP GCC for Arm Embedded Processors v10.2 build 1728.pngSorry for the inconvenience we bring you!


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

0 Kudos
Reply