Microsoft COM Automation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Microsoft COM Automation

2,751 Views
lishaoming
Contributor II

Whether there is the function like Microsoft COM Autionmation in  S32 Design Studio for Power Architecture ?

This feature exists in CodeWarrior.I want to implement it in S32 studio.

Labels (2)
0 Kudos
Reply
2 Replies

2,544 Views
stanish
NXP Employee
NXP Employee

Hello,

S32DS is multi-platform Development tool (Windows, Linux)

It is based on Eclipse (java) and therefore COM automation is not present in contrast to CodeWarrior Classic IDE.

You can possibly try to search an alternative solutions based on Eclipse IDE.

If you want to script in the debugger you can find this article useful:

Command Line Programming and Debugging with GDB | MCU on Eclipse 

Stan

0 Kudos
Reply

2,544 Views
lishaoming
Contributor II

Thank you for your answer.

I have learned the content of connecting the website. This is the system control method for PE debugger.

I want to control S32 Design Studio through Matlab, and it can be opened, compiled, and downloaded.

0 Kudos
Reply