MPC5775E CAN Communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5775E CAN Communication

3,371件の閲覧回数
bk13
Contributor III

Hello NXP Community,

I am trying to implement CAN communication on MPC5775E. My Transmite and Receive functions are as follows. While debugging, I see that it is stuck in the while loop inside the TransmitMsg function.

 

while ( CAN_A.IFLAG1.B.BUF31TO8I == 0) { } // wait until the tx is completed.

 

 

bk13_0-1676882692230.pngbk13_0-1676882692230.png 

bk13_1-1676882748516.pngbk13_1-1676882748516.png

 

Could you pelase help me how to solve these problems?

 

Best Regards,

 

Berfin.

5 返答(返信)

3,357件の閲覧回数
bk13
Contributor III

Hello @PetrS @martin_kovar,

I have studied your examples on this subject, but I could not solve these problems. Could you please help me?

 

Best Regards.

3,347件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this while statement is checking if MB flag is set, that is, if message is successfully transmitted without error.
So check that, if any error is detected (ESR1, ECR registers), check MB CODE field.
Do you have node (MPC5775E with active CAN transceiver) connected to any other node and bus properly terminated?  

BR, Petr

3,320件の閲覧回数
bk13
Contributor III

Hello,

I expect CAN communication to occur between the computer and the evaluation board. There is no other node in between and bus properly terminated. 

 

Best Regards

0 件の賞賛
返信

3,314件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

ESR1 cannot be zero if module is in Normal mode. At that case at least SYNC and IDLE bits should be set for free bus. So either you are not in normal mode or for example pins are not properly set. Check the MCR as well, if FZRACK and NOTRDY indicate normal mode, then you can try to disconnect TX/RX pins from transceiver and connect it together, to test pin setting. Send a message and you should get ACK error with TX error counter at 0x80 value. If this is true connect transceiver back and do the same with disconnecting from bus. You should get the same behavior as above.

BR, Petr 

 

0 件の賞賛
返信

3,344件の閲覧回数
bk13
Contributor III

Hello Petr,

Thank you so much for your help and interest. ESR1 and ECR registers are zero. 

bk13_0-1676898091421.pngbk13_0-1676898091421.png

MB Registers are as below. It seems to be true

bk13_1-1676898345488.pngbk13_1-1676898345488.png

Best Regards