MPC5748G-DEbugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,003件の閲覧回数
kalai
Contributor I

HI,

 

 

      do we need separate debugger for MPC5748.if yes please suggest 

 

 

thanks

kalai

0 件の賞賛
返信
1 解決策
1,995件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi kalai,

If you are using DEVKIT-MPC5748G board, then on board OpenSDA debugger is able to debug it.
For external debugger of MPC5748G, you can refer: I want to purchase a MPC5748G board, which debugger it supports

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,996件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi kalai,

If you are using DEVKIT-MPC5748G board, then on board OpenSDA debugger is able to debug it.
For external debugger of MPC5748G, you can refer: I want to purchase a MPC5748G board, which debugger it supports

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信