Issues about S32R274RRUEVB's reset escalation problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues about S32R274RRUEVB's reset escalation problem

1,577件の閲覧回数
445100643
Contributor I

Hi there:

I bought a S32R274RRUEVB daughter board and MPC57XXXMB mother board and tried to debug them with a PEMicro debugger.It is the first time I use them.

But when I plugged the daughter board to the mother board and turned the power switch on,I found the RESET LED D2 was always on no matter how many times I  pressed the reset switch on the daughter board.Then if I tried to debug the example included in S32DS,an error like this pop-up.

pastedImage_1.png

Did I miss anything or do anything wrong about this?I'm looking forward to your advice.Thank you!

Regards,

Junzhe

ラベル(2)
0 件の賞賛
返信
1 返信

1,518件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

what about power cycling the board - it doesn't help? Sometimes you need to be very fast - turn OFF power, turn it ON and almost instantly click on retry button on debugger connection error message. 

Hope it helps. 

Jiri 

0 件の賞賛
返信