Issue with the usage of Standalone tag in the ProjectStaticFilesGenerationMode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue with the usage of Standalone tag in the ProjectStaticFilesGenerationMode

1,786件の閲覧回数
satish_k_singh
Contributor III

Hello ,

I have changed the tag in the processorExpert.pe from <ProjectStaticFilesGenerationMode>Linked</ProjectStaticFilesGenerationMode> to <ProjectStaticFilesGenerationMode>STANDALONE</ProjectStaticFilesGenerationMode> and I see the below related to the missing inclusion of the header files during the build as can be seen in the second snapshot.

So could you please let know how should i incorporate the changed path in the make.

pastedImage_2.pngpastedImage_3.png

Thanks and best regards!!!

タグ(2)
0 件の賞賛
返信
4 返答(返信)

1,623件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please write me, which version of S32DS you use and which example did you try to switch?

Have you also seen the tutorial below:

https://community.nxp.com/docs/DOC-342838 

Regards,

Martin

0 件の賞賛
返信

1,623件の閲覧回数
satish_k_singh
Contributor III

Hello ,

I made the changes as mentioned above , but I still have the issue as the below files are not getting included during the compilation.

pastedImage_2.png

0 件の賞賛
返信

1,623件の閲覧回数
satish_k_singh
Contributor III

Hello ,

Sorry i Missed out to mention the version number , I make use of the version 2.0

pastedImage_2.png

0 件の賞賛
返信

1,623件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

I wanted to ask you about project, but I saw you created new thread and my colleague Jiri Kral posted you some answer.

https://community.nxp.com/thread/501563 

I followed the tutorial I shared above in S32DS 2.0 and it works correct on my side. You can try to clean project, generate SDK code and compile again.

Regards,

Martin