Issue with debug in S32DS v3.3 (S32G274)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with debug in S32DS v3.3 (S32G274)

1,322 次查看
Somasundaram_Vadivelu
Contributor III

I am trying to debug the code by setting breakpoints in the code, but I get this message:

Somasundaram_Vadivelu_0-1610100646740.png

Any help would be apperciated. Thanks

 

0 项奖励
回复
2 回复数

1,286 次查看
mikedoidge
NXP Employee
NXP Employee

Hello,

Could you please provide more details? What is displayed when you select the 'Details >>>' button?

It would also help if you could enable the following and then provide the log:

mikedoidge_0-1610398672635.png

In addition, check the document:

"C:\NXP\S32DS.3.3\S32DS\tools\S32Debugger\Debugger\scripts\s32g2xx\README.txt"

Ensure you are not exceeding the number specified for each type of breakpoint.

Best Regards,

Mike

0 项奖励
回复

1,297 次查看
liuxing_hu
Contributor III

liuxing_hu_0-1610358180109.png

you can try configuration as the above picture, I had similar issue before

0 项奖励
回复