Is building Fortran code available for MPC5748G?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is building Fortran code available for MPC5748G?

2,745件の閲覧回数
jlee4
Contributor II

Hi,

I'm investigating whether it is possible to build and run a Fortran project code  (BLAS/LAPACK, a famous matrix library) on MPC5748G; though MPC5748G officially supports either C or C++, I thought it is possible as S32DS, an IDE for the microcontroller, contains a Fortran compiler named `powerpc-eabivle-gfortran` but it has failed so far. I am just wondering if:

- I can build a Fortran code on S32S for MPC5748G

- If yes, I can run the resulting executable file on MPC5748G

I'm looking forward to answers or opinions from any pundits who are working on it and/or have relevant experience.

ラベル(3)
0 件の賞賛
返信
1 返信

2,726件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信