Is building Fortran code available for MPC5748G?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is building Fortran code available for MPC5748G?

2,740 Views
jlee4
Contributor II

Hi,

I'm investigating whether it is possible to build and run a Fortran project code  (BLAS/LAPACK, a famous matrix library) on MPC5748G; though MPC5748G officially supports either C or C++, I thought it is possible as S32DS, an IDE for the microcontroller, contains a Fortran compiler named `powerpc-eabivle-gfortran` but it has failed so far. I am just wondering if:

- I can build a Fortran code on S32S for MPC5748G

- If yes, I can run the resulting executable file on MPC5748G

I'm looking forward to answers or opinions from any pundits who are working on it and/or have relevant experience.

0 Kudos
Reply
1 Reply

2,721 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 Kudos
Reply