IRQ with processor expert

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IRQ with processor expert

1,347 Views
zhaoyanling
Contributor III

Hello expert,

My requirement is that : when pin2 of Port B input 0, then a gpio interrupt will be triggered. I do the configuration as following fig:

setting_1.bmp

I do not understand where can I set the IRQ callback function? the following codes are used for the whole pins of Port B, but I only want to pin2 of Port B to trigger interrupt, other pins of Port B are ignored. How can I do to set the pin2 of port B interrupt?

setting_2.bmp

So I met the problem : how can I generate  a gpio interrupt of one pin with processor expert of S32DS ? Could you help me again? Thank you very much!

0 Kudos
Reply
0 Replies