IRQ with processor expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IRQ with processor expert

1,310件の閲覧回数
zhaoyanling
Contributor III

Hello expert,

My requirement is that : when pin2 of Port B input 0, then a gpio interrupt will be triggered. I do the configuration as following fig:

setting_1.bmp

I do not understand where can I set the IRQ callback function? the following codes are used for the whole pins of Port B, but I only want to pin2 of Port B to trigger interrupt, other pins of Port B are ignored. How can I do to set the pin2 of port B interrupt?

setting_2.bmp

So I met the problem : how can I generate  a gpio interrupt of one pin with processor expert of S32DS Could you help me again? Thank you very much!

0 件の賞賛
返信
0 返答(返信)