IPCF - communicating between M core and A-Core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPCF - communicating between M core and A-Core

2,049件の閲覧回数
ggowdar
Contributor I

Hi Team,

               I am using the IPCF 2.1.1 and able to send data from A-core to M-core by following the IPCF user manual. 

just wondering how can I transfer data from M-core to A-core, currently I see from the user manual the procedure is for only A-core to M-core and check on the reply/echo messages.

is there any option to send a message from M-core to A-core in the same way as it is provided from A-core to M-core.

I am using S32G EVB board.

Appreciate your quick reply.

Thank You

0 件の賞賛
返信
1 返信

2,032件の閲覧回数
bpe
NXP Employee
NXP Employee

The procedure that sends an echo response in the available demo application for the M7 side is pretty generic and can be used independently of the incoming communication provided that the payload is generated locally instead of copying it from the received message.

 

Best Regards,
Platon

0 件の賞賛
返信