At first, I should let you know chip is S32K144, and it's a master. ADS1015 is slave address. Slave address is 0x4A.
I send four bytes to the IIC bus, first byte is slave address, second is register pointer. third and fourth are the parameters about the register in ADS.
But I use oscilloscope to get the wave form.it only send slave addr. Please see the following picture.


I find it receive the ACK signal. But In the default ISR, it shows that receive NACK.
But it can execute write operation. See the following picture.

The function I use is LPI2C_DRV_MasterSendData();
Can you give me some suggestions for this issue?
Thanks for your support firstly.
Best regards,
Xiaowei.