IAR Embedded Workbench Eclipse Plugin Problem In S32DS for ARM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IAR Embedded Workbench Eclipse Plugin Problem In S32DS for ARM

2,623件の閲覧回数
zhiwei1
Contributor I

Ask for help

I tried to configure IAR Plugin and encountered the following problems:

zhiwei1_0-1651197544828.png

 

0 件の賞賛
返信
3 返答(返信)

2,590件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi Zihwei,

It looks like the IAR plugin is requiring some Eclipse package which did not exist when S32 Design Studio for Arm was released. You will need to locate this package from http://download.eclipse.org site and install it.

Best Regards,

Mike

0 件の賞賛
返信

2,544件の閲覧回数
zhiwei1
Contributor I

Hi Mike,

What is the specific download address of "package org.eclipse.jdt.internal.eval 0.0.0",For example.When I need to download EMF, the download address is http://download.eclipse.org/modeling/emf/emf/builds/release/2.13.

0 件の賞賛
返信

2,537件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello Zhiwei,

Probably you should contact IAR for this information. It's possible the package is standard one on newer versions of Eclipse. You might want to check the release notes for the IAR plug-in to see which versions of Eclipse are supported. It's possible it is for a new version of Eclipse than the one you have installed with S32 Design Studio for Arm. Probably IAR could guide you to the correct plug-in version for the IAR compiler you wish to use and for the Eclipse version included with the S32 Design Studio for Arm version you've chosen.

Best Regards,

Mike

0 件の賞賛
返信