I want to send the received data to the computer again. I don't know what is wrong with the interrupt program.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I want to send the received data to the computer again. I don't know what is wrong with the interrupt program.

1,238件の閲覧回数
1416899748
Contributor I

The following is the code, mainly whether there is a problem with the interrupt program.

Also, I want to save the data received by CAN in EEPROM. Where should the data source be, RAMn?

/*
* main implementation: use this 'C' sample to create your own application
*
*/


#include "S32K144.h" /* include peripheral declarations S32K144 */
unsigned char LED_COUNT;

#define LED_ON() (PTD->PDOR |= (1<<12))
#define LED_OFF() (PTD->PDOR &= ~(1<<12))
uint32_t RxCODE; /* Received message buffer code */
uint32_t RxID; /* Received message ID */
uint32_t RxLENGTH; /* Received message number of data bytes */
uint32_t RxDATA[2]; /* Received message data (2 words) */
uint32_t RxTIMESTAMP; /* Received message time */


void LPIT0_init (void)
{
PCC->PCCn[PCC_LPIT_INDEX] = PCC_PCCn_PCS(6); // LPIT0时钟 Clock Src = 6 (SPLL2_DIV2_CLK=160MHZ/4 = 40MHZ)
PCC->PCCn[PCC_LPIT_INDEX] |= PCC_PCCn_CGC_MASK; //使能LPIT0时钟
LPIT0->MCR = 0x00000001; // DBG_EN-0: 当设备进入调试模式停止计时器
// DOZE_EN=0: 当设备进入睡眠模式停止计时器
// SW_RST=0: 计时器通道和寄存器未重置
// M_CEN=1: 启用外围时钟定时器
LPIT0->MIER = 0x00000001; // TIE0=1: 定时器LPIT 通道0启动中断
LPIT0->TMR[0].TVAL = 4000000; // 定时器值寄存器: 4M clocks
LPIT0->TMR[0].TCTRL = 0x00000001; // T_EN=1: 定时器启动
}

void LPIT0_NVIC_init_IRQs (void)
{
S32_NVIC->ICPR[1] = 1 << (48 % 32); /* IRQ48-LPIT0 ch0: clr any pending IRQ*/
S32_NVIC->ISER[(uint32_t)(LPIT0_Ch0_IRQn) >> 5U] = (uint32_t)(1UL << ((uint32_t)(LPIT0_Ch0_IRQn) & (uint32_t)0x1FU));
S32_NVIC->IP[48] = 0x8; /* IRQ48-LPIT0 ch0: priority 8 of 0-15*/
}
void WDOG_disable (void)
{
WDOG->CNT=0xD928C520; //解锁看门狗
WDOG->TOVAL=0x0000FFFF; //把时间配置为最大
WDOG->CS = 0x00002100; //关闭看门狗
}
void SOSC_init_8MHz(void)
{
SCG->SOSCDIV=0x00000101; //SOSCDIV1 & SOSCDIV2 =1: 分频/1
SCG->SOSCCFG=0x00000024; //Range=2: 选择晶体振荡器的中频范围 (SOSC 1MHz-8MHz)
// HGO=0: 控制晶体振荡器的工作功率模式 --低功率模式
// EREFS=1: 外部参考选择OSC内部晶体振荡器
while(SCG->SOSCCSR & SCG_SOSCCSR_LK_MASK); //等待SOSCCSR解锁 寄存器解锁后才可写入
SCG->SOSCCSR=0x00000001; // LK=0: SOSCCSR可以写
// SOSCCM=0: 系统OSC时钟监视器被禁用
// SOSCEN=1: 启用系统OSC
while(!(SCG->SOSCCSR & SCG_SOSCCSR_SOSCVLD_MASK)); //等待系统OSC成功启用,输出时钟有效
}


void SPLL_init_160MHz(void)
{
while(SCG->SPLLCSR & SCG_SPLLCSR_LK_MASK); //等待SPLLCSR寄存器解锁 寄存器解锁后才可写入
SCG->SPLLCSR = 0x00000000; // LK=0: SPLLCSR可以写入
// SPLLEN=0: SPLL禁用
SCG->SPLLDIV = 0x00000302; // SPLLDIV1 分频/2; SPLLDIV2 分频/4
SCG->SPLLCFG = 0x00180000; // PREDIV=0: 锁相环参考时钟分频因子
// MULT=24: SPLL时钟频率的乘法因子
// SPLL_CLK = 8MHz / 1 * 40 / 2 = 160 MHz SPLL_CLK = (VCO_CLK)/2 VCO_CLK = SPLL_SOURCE/(PREDIV+1)*(MULT+16)
while(SCG->SPLLCSR & SCG_SPLLCSR_LK_MASK); //等待SPLLCSR寄存器解锁 寄存器解锁后才可写入
SCG->SPLLCSR = 0x00000001; // LK=0: SPLLCSR可以写入
// SPLLCM=0: SPLL时钟监视器被禁用
// SPLLEN=1: 开启SPLL
while(!(SCG->SPLLCSR & SCG_SPLLCSR_SPLLVLD_MASK)); //等待SPLL成功启用,输出时钟有效
}

void NormalRUNmode_40MHz (void)
{
SCG->RCCR=SCG_RCCR_SCS(6) // SPLL做为系统时钟源
|SCG_RCCR_DIVCORE(0b11) // DIVCORE=3, 分频/4: Core clock = 160/4 MHz = 40 MHz
|SCG_RCCR_DIVBUS(0b11) // DIVBUS=3, 分频/4: bus clock = 160/4 MHz = 40 MHz
|SCG_RCCR_DIVSLOW(0b111); // DIVSLOW=7, 分频/8: SCG slow, flash clock= 160/8 MHz = 20MHZ
while (((SCG->CSR & SCG_CSR_SCS_MASK) >> SCG_CSR_SCS_SHIFT ) != 6) {}//等待系统时钟源成功选择SPLL
}

void GPIO_Init(void)
{
/*******输出端口配置*******/
PCC->PCCn[PCC_PORTE_INDEX] |= PCC_PCCn_CGC_MASK; //使能PTE端口时钟
PCC->PCCn[PCC_PORTD_INDEX] |= PCC_PCCn_CGC_MASK; //使能PTD端口时钟
PTE->PDDR |= (1<<16); //配置PTE16为输出端口
PTD->PDDR |= (1<<0); //配置PTD0为输出端口
PTD->PDDR |= (1<<1); //配置PTED1为输出端口
PTD->PDDR |= (1<<14); //配置PTED14为输出端口
PTD->PDDR |= (1<<15); //配置PTED15为输出端口
PTD->PDDR |= (1<<16); //配置PTED16为输出端口
PTE->PDDR |= (1<<9); //配置PTE9为输出端口
PTE->PDDR |= (1<<11); //配置PTE11为输出端口
PTE->PDDR |= (1<<15); //配置PTE15为输出端口


PORTE->PCR[16] = 0x00000100; //配置PTE16为GPIO,不使用其他复用功能
PORTD->PCR[0] = 0x00000100; //配置PTD0为GPIO,不使用其他复用功能
PORTD->PCR[14] = 0x00000100; //配置PTD14为GPIO,不使用其他复用功能
PORTD->PCR[15] = 0x00000100; //配置PTD15为GPIO,不使用其他复用功能
PORTD->PCR[16] = 0x00000100; //配置PTD16为GPIO,不使用其他复用功能
PORTD->PCR[1] = 0x00000100; //配置PTD1为GPIO,不使用其他复用功能
PORTE->PCR[9] = 0x00000100; //配置PTE11为GPIO,不使用其他复用功能
PORTE->PCR[11] = 0x00000100; //配置PTE11为GPIO,不使用其他复用功能
PORTE->PCR[15] = 0x00000100; //配置PTE15为GPIO,不使用其他复用功能

PTE->PDOR |= 1<<16; //PTE16输出高电平 DO4 DO5 DO6 DO7更改状态使能
PTD->PDOR &= ~(1<<0); //PTD0输出低电平
PTD->PDOR &= ~(1<<14); //PTD14输出低电平
PTD->PDOR &= ~(1<<15); //PTD15输出低电平
PTD->PDOR &= ~(1<<16); //PTD16输出低电平
PTD->PDOR &= ~(1<<1); //PTD1输出低电平
PTE->PDOR &= ~(1<<9); //PTE9输出低电平
PTE->PDOR &= ~(1<<11); //PTE11输出低电平
PTE->PDOR &= ~(1<<15); //PTE15输出低电平


/*******输入端口配置******/
PCC->PCCn[PCC_PORTB_INDEX] |= PCC_PCCn_CGC_MASK; //使能PTB端口时钟
PTB->PDDR &= ~(1<<4); //配置PTB4为输入端口
PTB->PDDR &= ~(1<<5); //配置PTB5为输入端口
PTD->PDDR &= ~(1<<13); //配置PTD13为输入端口
PTE->PDDR &= ~(1<<8); //配置PTE8为输入端口
}

void CAN0_PORT_init (void)
{

PCC->PCCn[PCC_PORTC_INDEX] |= PCC_PCCn_CGC_MASK; //使能PTC端口时钟
PORTC->PCR[2] |= PORT_PCR_MUX(3); // Port C2: MUX = ALT5, CAN0_RX 复用
PORTC->PCR[3] |= PORT_PCR_MUX(3); // Port C3: MUX = ALT5, CAN0_TX 复用

PCC->PCCn[PCC_PORTD_INDEX] |= PCC_PCCn_CGC_MASK; //使能PTD端口时钟
PTD->PDDR |= (1<<7); //端口PTD7配置为输出
PORTD->PCR[7] = 0x00000100; //端口PTD7为GPIO
//PTD->PDOR |= 1<<7; //输出高电平
PTD->PTOR &= ~(1<<7); //输出低电平
}
void CAN1_PORT_init (void)
{
PCC->PCCn[PCC_PORTA_INDEX] |= PCC_PCCn_CGC_MASK; //使能PTA端口时钟
PORTA->PCR[12] |= PORT_PCR_MUX(3); // Port C2: MUX = ALT5, CAN0_RX 复用
PORTA->PCR[13] |= PORT_PCR_MUX(3); // Port C3: MUX = ALT5, CAN0_TX 复用


PTA->PDDR |= (1<<14); //端口PTA14配置为输出
PORTA->PCR[14] = 0x00000100; //端口PTBA14为GPIO
PTA->PTOR |= 1<<14; //输出高电平
//PTA->PTOR &= ~(1<<14); //输出低电平
}
void CAN2_PORT_init (void)
{
PCC->PCCn[PCC_PORTC_INDEX] |= PCC_PCCn_CGC_MASK; //使能PTC端口时钟
PORTC->PCR[16] |= PORT_PCR_MUX(3); // Port C2: MUX = ALT5, CAN0_RX 复用
PORTC->PCR[17] |= PORT_PCR_MUX(3); // Port C3: MUX = ALT5, CAN0_TX 复用


PTC->PDDR |= (1<<15); //端口PTC15配置为输出
PORTC->PCR[15] = 0x00000100; //端口PTC15为GPIO
PTC->PTOR |= 1<<15; //输出高电平
//PTC->PTOR &= ~(1<<15); //输出低电平
}
void FLEXCAN0_init(void) {
#define MSG_BUF_SIZE 4 /* Msg Buffer Size. (CAN 2.0AB: 2 hdr + 2 data= 4 words) */
uint32_t i=0;

PCC->PCCn[PCC_FlexCAN0_INDEX] |= PCC_PCCn_CGC_MASK; /* CGC=1: enable clock to FlexCAN0 */
CAN0->MCR |= CAN_MCR_MDIS_MASK; /* MDIS=1: Disable module before selecting clock */
CAN0->CTRL1 &= ~CAN_CTRL1_CLKSRC_MASK; /* CLKSRC=0: Clock Source = oscillator (8 MHz) */
CAN0->MCR &= ~CAN_MCR_MDIS_MASK; /* MDIS=0; Enable module config. (Sets FRZ, HALT)*/
while (!((CAN0->MCR & CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT)) {}
/* Good practice: wait for FRZACK=1 on freeze mode entry/exit */
CAN0->CTRL1 = 0x00DB0006; /* Configure for 500 KHz bit time */
/* Time quanta freq = 16 time quanta x 500 KHz bit time= 8MHz */
/* PRESDIV+1 = Fclksrc/Ftq = 8 MHz/8 MHz = 1 */
/* so PRESDIV = 0 */
/* PSEG2 = Phase_Seg2 - 1 = 4 - 1 = 3 */
/* PSEG1 = PSEG2 = 3 */
/* PROPSEG= Prop_Seg - 1 = 7 - 1 = 6 */
/* RJW: since Phase_Seg2 >=4, RJW+1=4 so RJW=3. */
/* SMP = 1: use 3 bits per CAN sample */
/* CLKSRC=0 (unchanged): Fcanclk= Fosc= 8 MHz */
for(i=0; i<128; i++ ) { /* CAN0: clear 32 msg bufs x 4 words/msg buf = 128 words*/
CAN0->RAMn[i] = 0; /* Clear msg buf word */
}
for(i=0; i<16; i++ ) { /* In FRZ mode, init CAN0 16 msg buf filters */
CAN0->RXIMR[i] = 0xFFFFFFFF; /* Check all ID bits for incoming messages */
}
CAN0->RXMGMASK = 0x1FFFFFFF; /* Global acceptance mask: check all ID bits */
CAN0->RAMn[ 4*MSG_BUF_SIZE + 0] = 0x04000000; /* Msg Buf 4, word 0: Enable for reception */
/* EDL,BRS,ESI=0: CANFD not used */
/* CODE=4: MB set to RX inactive */
/* IDE=0: Standard ID */
/* SRR, RTR, TIME STAMP = 0: not applicable */
//#ifdef NODE_A /* Node A receives msg with std ID 0x511 */
// CAN0->RAMn[ 4*MSG_BUF_SIZE + 1] = 0x14440000; /* Msg Buf 4, word 1: Standard ID = 0x511 */
//#else /* Node B to receive msg with std ID 0x555 */
CAN0->RAMn[ 4*MSG_BUF_SIZE + 1] = 0x15540000; /* Msg Buf 4, word 1: Standard ID = 0x555 */
//#endif
/* PRIO = 0: CANFD not used */
CAN0->MCR = 0x0000001F; /* Negate FlexCAN 1 halt state for 32 MBs */
while ((CAN0->MCR && CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT) {}
/* Good practice: wait for FRZACK to clear (not in freeze mode) */
while ((CAN0->MCR && CAN_MCR_NOTRDY_MASK) >> CAN_MCR_NOTRDY_SHIFT) {}
/* Good practice: wait for NOTRDY to clear (module ready) */
}

void FLEXCAN0_transmit_msg(void) { /* Assumption: Message buffer CODE is INACTIVE */
CAN0->IFLAG1 = 0x00000001; /* Clear CAN 0 MB 0 flag without clearing others*/
CAN0->RAMn[ 0*MSG_BUF_SIZE + 2] = 0xA5112233; /* MB0 word 2: data word 0 */
CAN0->RAMn[ 0*MSG_BUF_SIZE + 3] = 0x44556677; /* MB0 word 3: data word 1 */
//#ifdef NODE_A
CAN0->RAMn[ 0*MSG_BUF_SIZE + 1] = 0x15540000; /* MB0 word 1: Tx msg with STD ID 0x555 */
//#else
// CAN0->RAMn[ 0*MSG_BUF_SIZE + 1] = 0x14440000; /* MB0 word 1: Tx msg with STD ID 0x511 */
//#endif
CAN0->RAMn[ 0*MSG_BUF_SIZE + 0] = 0x0C400000 | 8 <<CAN_WMBn_CS_DLC_SHIFT; /* MB0 word 0: */
/* EDL,BRS,ESI=0: CANFD not used */
/* CODE=0xC: Activate msg buf to transmit */
/* IDE=0: Standard ID */
/* SRR=1 Tx frame (not req'd for std ID) */
/* RTR = 0: data, not remote tx request frame*/
/* DLC = 8 bytes */
}
void CAN0_NVIC_init_IRQs (void)
{
S32_NVIC->ICPR[1] = 1 << (81 % 32); /* IRQ81-CHA0 0-15: clr any pending IRQ*/
S32_NVIC->ISER[(uint32_t)(CAN0_ORed_0_15_MB_IRQn) >> 5U] = (uint32_t)(1UL << ((uint32_t)(CAN0_ORed_0_15_MB_IRQn) & (uint32_t)0x1FU));
S32_NVIC->IP[81] = 0xb; /* IRQ81-CAN0 0-15: priority 10 of 0-15*/
}
void LPIT0_Ch0_IRQHandler (void) //时间中断
{
LED_COUNT++;
if(LED_COUNT==5) //0.5秒
{
LED_ON();
}
else if(LED_COUNT==10)
{
LED_OFF();
LED_COUNT = 0;
}
LPIT0->MSR |= LPIT_MSR_TIF0_MASK; /* 清除中断标志*/
}

int main(void)
{
WDOG_disable(); //关闭看门狗
SOSC_init_8MHz(); //配置系统振荡器为外部8MHZ
SPLL_init_160MHz(); //使用SOSC 8MHZ配置SPLL 为160 MHz
NormalRUNmode_40MHz(); //配置系列时钟40MHz, 40MHz总线时钟

GPIO_Init();
CAN0_PORT_init ();
CAN1_PORT_init ();
CAN2_PORT_init ();
FLEXCAN0_init();
CAN0_NVIC_init_IRQs();

//for(;;)
//{
//}
FLEXCAN0_transmit_msg();

}

void CAN0_ORed_0_15_MB_IRQHandler(void)
{
unsigned char j;

if ((CAN0->IFLAG1 >> 4) & 1)
{

RxCODE = (CAN0->RAMn[ 4*MSG_BUF_SIZE + 0] & 0x07000000) >> 24; /* Read CODE field */
RxID = (CAN0->RAMn[ 4*MSG_BUF_SIZE + 1] & CAN_WMBn_ID_ID_MASK) >> CAN_WMBn_ID_ID_SHIFT ;
RxLENGTH = (CAN0->RAMn[ 4*MSG_BUF_SIZE + 0] & CAN_WMBn_CS_DLC_MASK) >> CAN_WMBn_CS_DLC_SHIFT;
for (j=0; j<2; j++) { /* Read two words of data (8 bytes) */
RxDATA[j] = CAN0->RAMn[ 4*MSG_BUF_SIZE + 2 + j];
}
RxTIMESTAMP = (CAN0->RAMn[ 0*MSG_BUF_SIZE + 0] & 0x000FFFF);

if((RxID==0x15540000)||(RxID==0x14880000))
{
FLEXCAN0_transmit_msg();
}

CAN0->IFLAG1 = 0x00000010; /* Clear CAN 0 MB 4 flag without clearing others*/
}
}

タグ(1)
0 件の賞賛
返信
0 返答(返信)