I am running opengl test program tutorial6_es20 based on bsp19.0 in s32v234evb, there is a problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I am running opengl test program tutorial6_es20 based on bsp19.0 in s32v234evb, there is a problem

1,243 次查看
783435100
Contributor III

hi


I am running the tutorial6_es20 based on bsp19.0 in s32v234evb. I have the following information, I am doing this?

root@s32v234evb:/opt/viv_samples/vdk# ./tutorial6_es20
[ 1280.300134] fsl_dcu 40028000.dcu: DCU: unable to allocate memory for <fb0> surface.
[ 1280.300138] detected fb_set_par error, error code: -12
[ 1280.312574] fsl_dcu 40028000.dcu: DCU: unable to allocate memory for <fb0> surface.
[ 1280.312577] detected fb_set_par error, error code: -12
[ 1] NOTICE: Flush cache for USER_POOL memory!
500 frames in 8372 ticks -> 59.723 fps
root@s32v234evb:/opt/viv_samples/vdk#

Thank you !

0 项奖励
回复
1 回复

1,094 次查看
mikedoidge
NXP Employee
NXP Employee

Hi 783435100@qq.com,

This is not the correct community to post S32V2 questions.

Moreover, we have stopped supporting S32V2 community group. But we still support S32V2 question using our ticketing system.

For future questions, please create the request at www.nxp.com/support using Support Requests option. Our experts will help you.

Thank you for understanding.

Best Regards,

Mike

0 项奖励
回复