I am running opengl test program tutorial6_es20 based on bsp19.0 in s32v234evb, there is a problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I am running opengl test program tutorial6_es20 based on bsp19.0 in s32v234evb, there is a problem

1,227件の閲覧回数
783435100
Contributor III

hi


I am running the tutorial6_es20 based on bsp19.0 in s32v234evb. I have the following information, I am doing this?

root@s32v234evb:/opt/viv_samples/vdk# ./tutorial6_es20
[ 1280.300134] fsl_dcu 40028000.dcu: DCU: unable to allocate memory for <fb0> surface.
[ 1280.300138] detected fb_set_par error, error code: -12
[ 1280.312574] fsl_dcu 40028000.dcu: DCU: unable to allocate memory for <fb0> surface.
[ 1280.312577] detected fb_set_par error, error code: -12
[ 1] NOTICE: Flush cache for USER_POOL memory!
500 frames in 8372 ticks -> 59.723 fps
root@s32v234evb:/opt/viv_samples/vdk#

Thank you !

0 件の賞賛
返信
1 返信

1,078件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi 783435100@qq.com,

This is not the correct community to post S32V2 questions.

Moreover, we have stopped supporting S32V2 community group. But we still support S32V2 question using our ticketing system.

For future questions, please create the request at www.nxp.com/support using Support Requests option. Our experts will help you.

Thank you for understanding.

Best Regards,

Mike

0 件の賞賛
返信