Following is the output of the size tool.
My question is: Why the sections below the .stack are all started from the address 0x0?
D:\code\BCM1x_A_Sample\Debug\BCM1x_A_Sample.elf :
section size addr
.interrupts 0x400 0x0
.flash_config 0x10 0x400
.text 0x16b90 0x410
.interrupts_ram 0x400 0x1ffe0000
.data 0xcf4 0x1ffe0400
.code 0x0 0x1ffe10f4
.bss 0x14e68 0x20000000
.heap 0x400 0x20014e68
.stack 0x400 0x2001ec00
.ARM.attributes 0x30 0x0
.debug_info 0x8776d 0x0
.debug_abbrev 0x8368 0x0
.debug_aranges 0x3868 0x0
.debug_ranges 0x38e0 0x0
.debug_macro 0x1f15c 0x0
.debug_line 0x21ca9 0x0
.debug_str 0xb5a6b 0x0
.comment 0xa0 0x0
.debug_frame 0xe57c 0x0
Total 0x1c91d5
Thanks firstly!
I can understand the size tool's help info.
But, my question is:
Why the following sections all start from the address 0x0?
.ARM.attributes 0x30 0x0
.debug_info 0x8776d 0x0
.debug_abbrev 0x8368 0x0
.debug_aranges 0x3868 0x0
.debug_ranges 0x38e0 0x0
.debug_macro 0x1f15c 0x0
 
					
				
		
 BlackNight
		
			BlackNight
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		These are pseudo (not real code) sections. the include debug information which won't occupy any memory on your device. The 0x0 is simply a pseudo start address.
I hop this helps,
Erich