How to start S32 Design S for PA 2017.R1 - Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to start S32 Design S for PA 2017.R1 - Linux

2,041 Views
riez0306
Contributor I

I installed S32 Design Studio for Power Architecture 2017.R1 on my ubuntu 16.04 LTS.

However, I couldn't find the execute file in the installed folder.

How can I start this app?

0 Kudos
Reply
3 Replies

1,961 Views
riez0306
Contributor I

Hi. Jiri.

Thank you for your reply.

I found

/home/user/NXP/S32DS_Power_v2017.R1/

directory. but, there is NOT eclipse/ folder.

Do I need to install eclipse before S32DS installation?

R.E.

0 Kudos
Reply

1,961 Views
jiri_kral
NXP Employee
NXP Employee

Hi,

looks that something went wrong during installation. Try to re-install again S32DS. 

Jiri

0 Kudos
Reply

1,961 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

by default is installation executable - s32ds located in /home/user/NXP/S32DS_Power_v2017.R1/eclipse directory. 


I'm not much familiar with Ubuntu Unity GUI, but there should be link on desktop. If not, just navigate to directory above and locate s32ds executable. 

Hope it helps. 

Jiri

0 Kudos
Reply