How to start S32 Design S for PA 2017.R1 - Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to start S32 Design S for PA 2017.R1 - Linux

2,042件の閲覧回数
riez0306
Contributor I

I installed S32 Design Studio for Power Architecture 2017.R1 on my ubuntu 16.04 LTS.

However, I couldn't find the execute file in the installed folder.

How can I start this app?

0 件の賞賛
返信
3 返答(返信)

1,962件の閲覧回数
riez0306
Contributor I

Hi. Jiri.

Thank you for your reply.

I found

/home/user/NXP/S32DS_Power_v2017.R1/

directory. but, there is NOT eclipse/ folder.

Do I need to install eclipse before S32DS installation?

R.E.

0 件の賞賛
返信

1,962件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi,

looks that something went wrong during installation. Try to re-install again S32DS. 

Jiri

0 件の賞賛
返信

1,962件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

by default is installation executable - s32ds located in /home/user/NXP/S32DS_Power_v2017.R1/eclipse directory. 


I'm not much familiar with Ubuntu Unity GUI, but there should be link on desktop. If not, just navigate to directory above and locate s32ds executable. 

Hope it helps. 

Jiri

0 件の賞賛
返信