How to solve the problem that example project can't be compiled?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to solve the problem that example project can't be compiled?

5,130件の閲覧回数
abcb
Contributor I
Hi everyone,
After I install S32DS.ARM.2018.R1, I install RTM SDK 3.0.0 online. And then download and install "S32 Design Studio for ARM v2018.R1 Update 11 with S32 SDK S32K1xx SR 3.0.2". Create the example project (Can_pal_s32k144),
I encounter the following problems:
1. No "Cross Settings" in C/C++ Build option
2. gcc is not found
Related pictures are as below:
1. No Cross SettingsCross Setting.jpg
2. Gcc path is specofied
gcc path.jpg
3. Example Project has errors
Example  Project.jpg
Thank You
ラベル(3)
タグ(4)
0 件の賞賛
返信
4 返答(返信)

4,940件の閲覧回数
happybaby8882
Contributor I

I encountered the similar problem, create a new project, generate code from PE, and build, then a lot of problems occur, probably the generated code is empty, but i don't know why.

0 件の賞賛
返信

4,996件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

actually I never saw such issue before. I tried reproduce it, but on my machine everything works okay. So, you can try uninstall and install S32DS again - if you require this old version.  

The latest S332DS version is - https://community.nxp.com/docs/DOC-345517 

Jiri 

0 件の賞賛
返信

4,996件の閲覧回数
abcb
Contributor I

Hi Jiri,

I've tried uninstall and install S32DS again, but the result is still the same.

Now I'm trying to install the latest S332DS version, hope there will be good news...

Thank you.

Adam Chiu

0 件の賞賛
返信

4,996件の閲覧回数
18062294269
Contributor I

hi

   I have the same problem ,have you    solved it ?

0 件の賞賛
返信