Hi,
I have attached .map file for one of the application.
From .map file I extracted below information.
Memory sections | Size in bytes |
.data | 2436 |
.text | 11320 |
.rodata | 48 |
.bss | 316 |
I would like to know how much RAM memory will be used when this application run on S32K144 MCU ?
Is there any provision in S32 design studio to monitor amount of RAM used when debugging this application on S32K144 evaluation board ?
Thanks
Mohan
Original Attachment has been moved to: S32K144_CSEC_KEYCONFIG_Example.map.zip
解決済! 解決策の投稿を見る。
Hi,
you can enable printing target size by right click on project name -> properties and check the Print size checkbox
In build console you can see something like this:
Here is detailed description of each block (text, data, bss...)
Jiri
Hi,
you can enable printing target size by right click on project name -> properties and check the Print size checkbox
In build console you can see something like this:
Here is detailed description of each block (text, data, bss...)
Jiri
Hi Jiri,
Thank you for the information.
From your experience can you please suggest how much of RAM is required in below scenario.
Use case Scenario:
a. freeRTOS
b. Load secure key to CSEc + Perform encryption and decryption on plain text using loaded secure key + Prepare for secure boot.
c. Run OBD CAN stack
d. Other hardware initialization if any
Thanks
Mohan
Hi,
well - I have no idea how many RAM your project will need - it depends on implementation. But I'm sure that 64kB of RAM on S32K144 is okay for your scenario.
Jiri
Hi Jiri,
Okay.
If you can share any sample project details like what all components were running on S32K144's 64K SRAM, it will be helpful to me.
Thanks
Mohan