How to integrate library file in a specific RAM area

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to integrate library file in a specific RAM area

1,502件の閲覧回数
WeoWang
NXP Employee
NXP Employee

Hi Dear Colleagues,

There is a requirement from my customer.

Their end customer gave them a library:

WeoWang_0-1675755062351.png

 

And required them to put the library into a specific RAM area,  then, use MPU to protect this area.

How to realize this requirement?

Best Regards

Weiyou Wang

0 件の賞賛
返信
1 返信

1,475件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Weiyou,

If the library source code has been compiled with custom sections attributes, then they can easily place these sections  (e.g. myLibConst) into custom memory space.

Anyway, gcc linker allows placement of any object code (.text) into a custom section. This way they could force to place library code/data/consts into a specitic memory custom sections even if the library object code was NOT compiled with specific placement for code/data/const.

see e.g.

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Run-a-routine-from-RAM-in-S32-De...

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Execute-a-library-function-from-...

 

Hope it helps.

Stan

0 件の賞賛
返信