How to flash the NXP S32G274A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to flash the NXP S32G274A

11,372件の閲覧回数
yihan_cheng
Contributor II

Hello,

I'm a software engineer, in our team we want to develop autosar project on S32G27A Plattform.

I downloaded the S32DS for Plattform and additional Packages for S32G. And Try to debug the example project "hello_world_s32g27a" on the S32G plattform.

Questions:

  1. What is the different between use S32G-PROCEVB-S standalone and stack S32G-PROCEVB-S on S32GRV-PLATEVB?
  2. Must I use a lauterbach or s32g debuger probe to debug a s32g project? can't i like FPGA plattform, simulate in software environement on my PC. then download code to Plattform?
  3. How can i flash my application on s32g plattform. I try to use usb connect my laptop and uart2usb port on plattform. the laptop recognize the COM18port, however when i use the flash tools. It said no device found.
  4. can i also use a SD card for linux boot on s32g plattform like the s32V234 board?
ラベル(1)
タグ(3)
8 返答(返信)

10,120件の閲覧回数
thaohm2
Contributor I

If you is working on this product of NXP, you may have the Trace32 package and probably figure out the flash scripts under below directory T32\demo\arm64\hardware\s32g2\s32g-vnp-evb\s32g-vnp-evb-m7-amp

0 件の賞賛
返信

10,120件の閲覧回数
thaohm2
Contributor I
If you is working on this product of NXP, you may have the Trace32 package and probably figure out the flash scripts under below directory T32\demo\arm64\hardware\s32g2\s32g-vnp-evb\s32g-vnp-evb-m7-amp
0 件の賞賛
返信

10,534件の閲覧回数
vinod_bargaje
Contributor II

Hello YIhan CHENG

Do you have .cmm (Lauterbach) script file for debugging and flashing S32G274a code ?

If you provide then it will be great help.

Thanks in advance

0 件の賞賛
返信

8,700件の閲覧回数
Sandeepu
Contributor I

Hi Vinod,

Sandeep here, I need S32G274A multicore .cmm (Lauterbach) file.

If you provide me it will be a great help.

 

Regards,

[email protected]

0 件の賞賛
返信

10,534件の閲覧回数
yihan_cheng
Contributor II

Hello Vinod,

I have no experience with lauterbach, however for the cmm files, you can download the source code from NXP software website (you need the access to the Automotive SW - S32G2 Standard Software).

In the Automotive SW - S32G2 Standard Software select the EVB DIAGONOSTIC TESTS

pastedImage_2.png

Then download the SW32G2-EVBDIAG-EAR-0.8.4, the cmm files is in the directory Tools\Scripts\cmm\Customer

RG
Yihan Cheng

10,534件の閲覧回数
vinod_bargaje
Contributor II

Appreciate [email protected] for your input. It solves my problem! 

Thanks Again. 

0 件の賞賛
返信

6,944件の閲覧回数
sreevishakh
Contributor II

Hi Vinod 

I am new to S32G board, need to make it up with adaptive autosar application. 

Can you brief the process to flash adaptive autosar application into it?

0 件の賞賛
返信

10,534件の閲覧回数
rweiss
Contributor V

Hi Vinod,

please contact Lauterbach support ([email protected]) for flash setup scripts.

Best regards,

Reinhard

0 件の賞賛
返信