How to build mpc5748g project under linux command line

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to build mpc5748g project under linux command line

2,160 Views
ningwang
Contributor III

      Hello,  I want to build the MPC5748g project under command line. This project can build in S32 studio IED(linux version), the IDE will create a DEBUD/ folder, and in command line(linux version) the project can be build. But if I don't have the DEBUG/ folder, how to generate the DEBUG/ or RELEASE/ under command line in linux, but not in windows?

      I ware that in the IDE, I can create a makefile project for the MPC5748g project, and gerenrate all the makefiles and args. I want to know how to use linux command line to create a makefile project for the existing projects? So I can get the Debug/ folder for all the make files.

      Where can I find the datasheet about how to use commands for building with the s32 studio tools?

     Thanks a lot.

0 Kudos
Reply
1 Reply

1,941 Views
ningwang
Contributor III

Do anyone know the method? Thanks very much!

0 Kudos
Reply