How to build demos in vision SDK for(under) build-x86-gnu-windows-d

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to build demos in vision SDK for(under) build-x86-gnu-windows-d

2,622 次查看
zhiwei_zhang1
Contributor I

hi experts:

     I want to using the apex emulation on windows.

     I  built the demo in vision SDK - demos\apps\pedestrian_detection_aggcf - successfully for  build-v234ce-gnu-linux-d .

But when I try to build it for build-x86-gnu-windows-d, many errors come out . 

1、According to the Makefile under build-x86-gnu-windows-d, I have built the opencv3.1.0 on my windows and get  the libopencv_xxx310.a file.

2、At the end of this Makefile , it includes the following files. but these files can not be found under SDK folder. Where can I find them ? or any workaround  ?

include $(DIR_SDK)/script/make/protected/config/build_config_x86_windows_gnu.min
include $(DIR_SDK)/script/make/protected/build_lib_rules.min
include $(DIR_SDK)/script/make/protected/build_app_rules.min
include $(DIR_SDK)/script/make/protected/build_targets.min

3、Following the Makefile under build-v234ce-gnu-linux-d, I change this Makefile, replace above includes with

   "include $(CURR_SDK_ROOT)/build/nbuild/platforms/$(notdir $(CURDIR))/Makefile" 

  and run "make allsub"

  It does not do any compile at all. --   make: Nothing to be done for `all'

There must be some way to build this demo on window. can you give any tips ?

标签 (1)
0 项奖励
回复
3 回复数

2,298 次查看
nxa22577
NXP Employee
NXP Employee

At the moment, we have not supported for x86-gnu-windows target in "demos\apps\pedestrian_detection_aggcf" and "demos\apps\pedestrian_detection" yet so you cannot compile it.

I hope in the next release we can support it.

Thank you for your response.

0 项奖励
回复

2,298 次查看
deliadong
Contributor I

Dear Xuyen,

Thanks for you reply.

Does demos\apps\pedestrian_detection support "apex emulation"?

Can the application run without the board?In other words, Can we build an executable file with the code, which can run on Linux or Windows?

0 项奖励
回复

2,298 次查看
zhiwei_zhang1
Contributor I

OK, Thanks.

0 项奖励
回复