How to add Processor Expert project to an existing project?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add Processor Expert project to an existing project?

3,273件の閲覧回数
songhengwang
Contributor I

Hello everyone,

Today is my first day to use S32 Design Studio for ARM v2.0, I want to add Processor Expert project to an existing project according to the help like picture below:

捕获1.JPG

But I can NOT find the Processor Expert folder, and my enviorment is like below:

捕获2.JPG

Can you please tell me the reason? I have checked the installing information, nothing abnormal.

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,822件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hello, 

the "New Wizard" screenshot is probably from older S32DS version. Processor expert is part of SDK and you can add Processor expert with SDK. Right click on your project name -> Properties 

pastedImage_1.png

Select SDKs and choose one which you are interested in and click on Attach button: 

pastedImage_2.png

Check for which configuration you like to use SDK (probably for all) 

pastedImage_3.png

and click on Apply and OK on Properties window. Processor expert should be ready for your project. 

Jiri 

0 件の賞賛
返信

2,822件の閲覧回数
songhengwang
Contributor I

Hello jiri,

Thanks for your fast answer! and my problem is solved according to your suggestion.

Thanks again!

Songheng

在 2017-12-04 17:21:54,"[email protected]" <[email protected]> 写道:

|

|

NXP Community

|

|

Re: How to add Processor Expert project to an existing project?

reply from Jiri Kral in S32 Design Studio - View the full discussion

Hello,

the "New Wizard" screenshot is probably from older S32DS version. Processor expert is part of SDK and you can add Processor expert with SDK. Right click on your project name -> Properties

https://community.nxp.com/servlet/JiveServlet/downloadImage/2-966605-205166/508-900/pastedImage_1.pn...

Select SDKs and choose one which you are interested in and click on Attach button:

https://community.nxp.com/servlet/JiveServlet/downloadImage/2-966605-205167/pastedImage_2.png

Check for which configuration you like to use SDK (probably for all)

https://community.nxp.com/servlet/JiveServlet/downloadImage/2-966605-205168/pastedImage_3.png

and click on Apply and OK on Properties window. Processor expert should be ready for your project.

Jiri

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in S32 Design Studio by email or at NXP Community

Following Re: How to add Processor Expert project to an existing project? in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

|

|

0 件の賞賛
返信